ECAT.RXDONETIME

Description

This parameter allows viewing and recording of the Distributed Clock (DC) time when the drive completes processing the output packet (RxPDO). The SM2 event happened a short time before this time.

Context

See Synchronization.

Versions

Action Version Notes
Implemented 02-06-01-000

General Information

Type

Read Only

Units

ns

Range

0 to 4,294,967,295 ns

Default Value

N/A

Data Type

Integer
See Also ECAT.RXIRQTIME ECAT.POSLOOPTIME, ECAT.TXDONETIME, ECAT.SYNC0TIME

Stored in Non-Volatile Memory

No

Variants Supported

EtherCAT variants: AKD2G-SPE

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

ECAT.RXDONETIME

4300h

02h

Unsigned32

-

-

Read only

Yes